Sub-devices management
A user needs to have VPN permissions on a device to add or delete sub-devices, change their settings, and manage the services that they provide.
- In theFactoryTalk Remote Access Manager, access the section.
- Select a sub-device in the domain (left) pane.Two information panels appear on the right pane:
- The sub-device information pane includes itsIP Address.
- TheServicespane shows a list with the sub-device services. You can add, edit or delete a service.NOTE: See Add a service to learn more on this subject.
- Once you select a sub-device, you can:
- Run the device by clickingLaunchin theServicespane.
- Click
to remove a sub-device.
Provide Feedback