Launch a service
You can launch a sub-device service through a specific
Services
section in the FactoryTalk Remote Access Manager
.- In, select the sub-device.
- On the right pane, expand the theServicessection to view all of the sub-device services.
- Select the service that you want to initiate and clickLaunch.TheInteractive AccessTool automatically establishes a VPN connection with the device to which the sub-device is connected. In this way, you are granted access to the device subnet, so you can reach the sub-device and make its service run.
Provide Feedback