Find in Controller Organizer command
Access the Find in Controller Organizer command
- From theLogical Organizer, right-click a program or routine, and selectFind in Controller Organizer.
Use the
Find in Controller Organizer
command to navigate from a program or routine in the Logical Organizer
to the same program or routine in the Controller Organizer
. For additional navigation information, see:
Provide Feedback