- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Alarm conditions for PDOSE
Use the
Alarms
tab on the PDOSE Properties
dialog box to define alarm conditions for Process Dosing (PDOSE) instructions.To define alarm conditions for PDOSE instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- SelectAlarms.
- Configure these settings:
- Use Alarm. Select to use the alarm. Alarm conditions are not evaluated when an alarm is not in use.
- Alarm. Enter descriptive text that appears for the alarm.
- Limit. For flow rate alarms, enter the flow rate threshold for raising the corresponding alarm in engineering units.
- State. The state of the alarm. Hover over the state icon to see a tool tip that describes the alarm state or fault status.An alarm can be in more than one state at a time. For example, an alarm can be in alarm, unacknowledged and suppressed; or it can be normal, acknowledged and shelved.Alarm state icons include:
- Normal, acknowledged (no icon).
- Normal, unacknowledged -
- In alarm, acknowledged -
- In alarm, unacknowledged -
- Suppressed -
- Shelved -
- Disabled -
- Alarm fault -
- To open theAlarm Propertiesdialog box for an alarm, select theConfigurationicon
.
- To configure settings for all pre-defined alarms for a PDOSE instruction, selectSettings for all alarms. When this box is checked, changes made to these settings are applied to all pre-defined alarms:
- Class. A group name for related alarms. The class does not limit the alarms that an Alarm Summary object subscribes to. UseClassto filter the alarms that are displayed to the operator.
- Alarm group. A group name to help classify and sort alarms.
- . AFactoryTalk ViewcommandFactoryTalk Viewcommand that can be run on the operator station when the alarm notification appears. Enter the exact syntax for theFactoryTalk Viewcommand.
- To allow an operator to shelve an alarm, selectAllow operator to shelve alarm.
- To allow maintenance technicians to disable an alarm, selectAllow maintenance to disable alarm.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. When theLogix Designerapplication is online with the controller, displays the current device state.
- Device issues. When theLogix Designerapplication is online with the controller, displays fault conditions.
- SelectApply.
Provide Feedback