HMI navigation for PDOSE
Use the
HMI Navigation
tab on the PDOSE Properties
dialog box to enable or disable navigation to the Quantity input or Rate input objects from the HMI faceplate for PDOSE instructions.To enable HMI navigation to Quantity input or Rate input objects for PDOSE instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectNavigation.
- To allow navigation to the Quantity input or Rate input objects from the HMI faceplate, selectAllow navigation.
- In theObject tag namebox, enter the name of the object.
- SelectApply.
Provide Feedback