Input Configuration Tab - FLEX I/O Analog

Use this tab to configure each input channel of your module. Some modules have a more detailed method used in their configuration. Select one of the following modules for more detailed configuration information.
Input
Output
Combo
Parameters
Voltage/Current Range
Select the voltage/current range and data format for each channel.
Conversion Rate
Select a rate at which to convert data from analog to digital (A/D) for each channel. The valid rates are: 150 Hz, 300 Hz, 600 Hz, or 1200 Hz.
Low Pass Time Constant
Select a low pass filter option for each input channel. The valid options are: 100 ms, 500 ms or 1000 ms.
low pass filter
A digital device that provides noise rejection for input signals. This device is programmable and has eight filter frequency options for each channel. A low frequency provides the most noise rejection. A high frequency provides the least noise rejection and a faster step response time.
Real Time Sample
The rate at which the module collects the most recent output of the converter that is later sent off to the adapter. Select a value in milliseconds. The valid range is 0-30000 in 5 ms intervals.
Interleave Module Interrupts
Do not check the Interleave Module Interrupts check box unless you know you have a specific use for this option. The Interleave Module Interrupts feature is useful only in limited circumstances and can only be enabled when you configured a module’s Conversion Rate to 1200 Hz, Low Pass Time Constant to None, and Real Time Sampling period to 0 for ALL channels on the module.
OK
Click this button to accept your edits on all tabs and close the dialog.
Cancel
Click this button to delete your edits on any tab and close the dialog.
Apply
Click this button to make your edits effective on any tab and continue editing.
TIP:
The connection to a FLEX I/O module using Rack communication cannot be inhibited. The
Inhibit
check box on the Connection tab is disabled in this case.
Help
Click this button for assistance with this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.