Associate an axis to a drive

Associate the drive is the first step in configuring the axis. The drive determines what optional attributes are supported.
To associate an axis to a drive:
  1. From the
    Axis Properties
    dialog box, in
    Categories
    , click
    General
    .
  2. In the
    Associated Module
    area, from the
    Module
    list, select the drive module you want to associate with the axis.
  3. From the
    Axis Number
    list, select the axis number.
  4. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.