Manual Tune page
Use the parameters in the
Manual Tune
page to manually tune the gains for optimum performance. Use the motion generator parameters to move the axis to test changes to the servo loop parameters.
NOTE:
Manual tuning is only available for Position Loop and Velocity Loop application types.
Manual Tune parameters
Parameter | Description |
---|---|
Reset | Returns the values to the state they were in at the time the dialog box opened. This only resets values on this dialog box. |
System Bandwidth | Type a value or move the slider to enter the overall bandwidth of the drive's servo loop. |
System Damping | Type a value or move the slider to enter the overall damping of drive's servo loop. Valid values are in the range of 0.5 to 2.0. The slider forces the value into the range of 0.8 to 1.5. |
Tuning Configuration | Click + to display the current Application Type , Coupling and Gains to Tune settings.
|
Position Loop | The Position Loop parameters are available when the Axis Configuration on the General page is set to Position Loop . |
Loop Bandwidth | Select a value for the loop bandwidth for the position loop. Valid values are in the range of 0 to Max Float. |
Integrator Bandwidth | Select a value for the integrator bandwidth for the position loop. Valid values are in the range of 0 to Max Float. |
Integrator Hold | Select whether to enable or disable the integrator hold for the velocity loop. |
Error Tolerance | Select a value for the error tolerance for the position loop. Valid values are in the range of 0 to Max Float. |
Velocity Loop | The Velocity Loop Parameters are available when the Axis Configuration on the General page is set to Velocity Loop . |
Loop Bandwidth | Select a value for the integrator bandwidth for the velocity loop. Valid values are in the range of 0 to Max Float. |
Integrator Bandwidth | select a value for the integrator bandwidth for the velocity loop. Valid values are in the range of 0 to Max Float. |
Integrator Hold | Select whether to enable or disable the integrator hold for the position loop. |
Error Tolerance | Select a value for the error tolerance for the velocity loop. Valid values are in the range of 0 to Max Float. |
Additional Tune Panel | Select to configure the feedforward, compensation, filters, limits, planner, and adaptive tuning options, and torque notch, torque, and command notch filters. |
Motion Generator parameters
Parameter | Description |
---|---|
Commands | Displays list of supported Motion Direct commands. |
More Commands | Select to open the Motion Direct Command dialog box to execute specific motion instructions while online. |
Danger | Display a warning message. |
Instruction Status | Displays the Motion Direct Command execution status (execution error). |
Safe Torque Off bypassed | Displays warning when the drive is a CIP Safety drive and the Safety State is Not Configured (Torque Permitted) or Not Running (Torque Permitted) . |
Axis State | Displays the state of the axis. For CIP axis, this control is associated with the CIP Axis State attribute. This parameter is available in online mode. |
Safety State | Displays the state of the CIP Safety drive. This parameter is available when the drive is a CIP Safety drive and in online mode. |
Axis Fault | Displays the fault state of the axis. The parameter is available in online mode. |
Start Inhibited | Displays the current state that inhibits the axis from starting. |
Execute | Used to execute the selected Motion Direct Command. The button is available in online mode. |
Disable Axis | Used to send a disable axis direct command to the controller. This button is available in online mode. |
Additional Tune | Displays additional tuning attributes. |
Provide Feedback