Select a Drive NV as the data source

The Drive NV data source derives motor attributes from the nonvolatile memory of a drive.
To select Drive NV as the data source:
  1. From the
    Axis Properties
    dialog box, in
    Categories
    , click
    Motor
    .
  2. In the
    Motor Device Specification
    area, in the
    Data Source
    list, click
    Drive NV
    .
  3. In the
    Units
    list, click the motor units that are associated with the motor.
    Tip:
    For a rotary motor, select
    Rev
    . For a linear motor, select
    Meter
    .
  4. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.