Command a transition using the Equipment Sequence Monitor
You can force an active transition to evaluate TRUE, STOPPING and RESETTING the preceding steps while attaching and STARTING the following steps.
Before you begin:
- Go online with the controller.
- In theEquipment SequenceMonitor, open anEquipment Sequence.
- TheEquipment Sequenceshould be running.
- The transition must be active.
- TheEquipment Sequencemust be inAutomaticmode.
To command a transition using the
Equipment Sequence
Monitor:- Select to take ownership of theEquipment Sequence.
- Right click on the transition and selectForce Expression to True.
Provide Feedback