Commanding and Running Equipment Sequences

The right to command an Equipment Sequence or an Equipment Phase is granted through ownership.
Both
Equipment Sequence
s and
Equipment Phase
s must be owned to be commanded. The ownership commands are Attach (SATT) and Detach (SDET).
Internal sequencers (programs), external sequencers (
FactoryTalk Batch
), and operators always use an Attach instruction to command an
Equipment Sequence
.
Logix Designer
always uses an Override instruction to command an
Equipment Sequence
. A program might successfully attach an
Equipment Sequence
but be unable to command it because
Logix Designer
has overridden ownership.
Once ownership is taken, steps and transitions can be commanded and
Equipment Sequence
s can be controlled.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.