Set ID button

The
Set ID
button assigns the user-specified sequence ID to the
Equipment Sequence
. You can only set the sequence ID when the following prerequisites are met:
  • The controller is online.
  • The
    Equipment Sequence
    is in the IDLE state.
  • You have taken ownership of the
    Equipment Sequence
    .
The sequence ID can be up to 82 characters in length, using the printable ASCII characters below:
a-z, A-Z, 0-9, !"#$%&'()*+,-./:;<=>?@[\] ^_`{|}~ and space
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.