Data Source Onboarding Automation

This automation process helps the customer to onboard data sources to bring data into CDF project for future/real-time uses. AI application can consume this data from CDF to perform various activities such as KPI calculations, batch comparison etc.
The data source onboarding feature of AI application enables the engineer to generate configuration files that are used by CDF extractors.
The CDF extractors configured in customer environment is responsible for bringing data into CDF from defined source.
AI application allows user to onboard two types of data sources:
  • PI/FT Historian
  • OPC UA
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.