OPC UA
Perform the following steps to register OPC UA data source:
- On the left navigation panel, underConfigurationdrop-down clickData Source Onboard.
- In theSelect Data Sourcetab, from theSelect Timeseries Extractordrop-down, selectOPC UA, and clickNext.Onboarding Data Source
- UnderData Source Configurationtab, provide the following parameters and clickNext:
- OPC UA endpoint URL
- Site
- Area
Data Source ConfigurationResult: The application sets up the required configuration and objects on Cognite and DataMosaix platforms and"Your registration is completed"message is displayed on successful registration of the data source.Registration Completed - To download the extractor configuration, clickClick to Open Config.yml fileand then clickDownload.Download Extractor Configuration File
- The user can copy the configuration template. To copy the template, clickCopy.
- ClickStart Overto start the onboarding process again orExitto go back to the home screen.
NOTE:
If registration fails, "
Your registration failed
" message is displayed. Provide Feedback