Runtime entitlements and feature tokens for target devices

Runtime entitlements differ between target devices.
Target device entitlements and feature tokens
Device type
Pre-assigned entitlement
Upgrade available
Maximum entitlement
Edge Compute
XS
5 feature tokens
Yes
L
15 feature tokens
OptixPanel
Compact
S
8 feature tokens
Yes
M
11 feature tokens
OptixPanel
Standard
M
11 feature tokens
Yes
L
15 feature tokens
ASEM
6300 Industrial PCs
none
No
XL
21 feature tokens
TIP:
If you need to purchase additional entitlements for an
ASEM
6300 device, remove the existing entitlement from the device and place it back on the Optix Portal. You can then purchase a new entitlement of a different size. You can reuse the previous entitlement on another device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.