The runtime sizing tool lets you enter the details of your project and recommends the feature token package that you need. The available packages include two options of each Station Runtime-Lite, Station Runtime-Standard, and Station Runtime-Pro.
To determine the runtime package that you need for your application, use the Runtime Sizing tool within the
FactoryTalk® Optix™
page.
Select
FactoryTalk® Optix™
from the list of available applications.
Select Runtime Sizing from the top navigation bar.
Follow the wizard to select the features your application needs.
For example, if you select these features:
Example sizing selections
Wizard Category
Example Selection
Select presentation
Web HMI Client
Select features
Data Logger
Database
Controller connections
Rockwell EtherNet/IP
Single connection
Rockwell Hardware
Select interoperability
OPC UA Client None
OPC UA Server 1 token
You see these recommended runtime packages:
Example recommended runtime packages
Select the package you want to see the associated catalog number for purchase via the Commerce Portal.