Safety Application Protection

Safety Application Protection

Use the Safety Lock feature to lock a Safety application to prevent further modification once you have verified that it is working as intended.
Certain software restrictions apply whenever a Safety application is in a Safety Secured state. This state occurs whenever one or more of the following conditions exist.
  • The Safety application is Locked.
  • A Safety signature exists.
  • A non-recoverable Safety fault is present.
  • The safety status is any value other than "Safety Task OK".
Whenever any of these conditions exist, the following software restrictions apply:
  • You cannot modify any Safety component, including the Safety task, Safety programs, Safety routines, Safety tags, Safety I/O modules, and tag mappings.
  • In cases where a relationship exists between a standard tag and a Safety tag, you cannot modify the standard tag.
  • You cannot edit the controller name, description, slot number, and chassis size.
  • If the controller has an embedded Ethernet port, you cannot modify the IP settings or IP address.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal