Create a trend
Create a trend to graphically plot sampled data onto a chart for up to eight tags.
To create a trend:
- Enter a name for the trend.
- Enter a description for the trend.
- If you wish to use a sample period that differs from the default sample period, enter a new sample period value.
- SelectOK.The trend is displayed in theTrendsfolder in theController Organizertree.
Provide Feedback