Open a trend chart
Open the chart for the selected trend to run the trend, access the trend chart properties, view setup information, and view sampled data for configured tags.
There are several ways to open a chart from the
Controller Organizer > Assets > Trends
folder:- Select the trend and pressEnter.
- Select the trend and chooseLogic>Openfrom the main menu.
- Right-click the trend and chooseOpen Chart.
- Double-click the trend.
Provide Feedback