Default Roles

Default Roles

There are seven predefined roles. These are designed to give a starting point for an implementation. The following table displays the list of default Roles and the associated capability groups.
Default Roles and Capability Groups
Default Role name
Default Capability Groups
Application Developer
FTDM-Grp-Applications
Applications
FTDM-Grp-GenApplications, FTDM-Grp-Experimental-Machine
Application User
FTDM-Grp-ViewApp
Data Configurator
FTDM-Grp-DataSetsManagement, FTDM-Grp-Function, FTDM-Grp- Pipeline, FTDM-Grp-DataModel
Data Scientist
FTDM-Grp-ContextDiag, FTDM-Grp-3D, FTDM-Grp-Data, FTDM-Grp-Raw, FTDM-Grp-Chart, FTDM-Grp-Media, FTDM-Grp-Experimental-Human, FTDM-Grp-ContextEntity
Extractors
FTDM-Grp- Extractor
Project Admin
FTDM-Grp-Project FTDM-Grp-CognlteApllnputValidations, FTDM- Grp-AccessManagement
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.