- Extractors
- Analyze Data
Custom Role
If the default role does not fulfill your requirements, you can create a custom role to suit your needs. Once the customized roles are created, to which corresponding default/custom groups can be assigned. Refer to Create a Custom Role.
NOTE:
Only the Project admin can create custom roles. Default roles are read-only.
Provide Feedback