How to set permissions rights
Once you have
invited a user to join your organization and set domain roles
, you can set user permissions rights.
NOTE:
See Create an organization and a domain and Domain roles and domain groups for more information on this subject.
- InFactoryTalk Remote Access Managerselect .
- In the left pane, select the folder or device for which you wish to set user permissions, then access thePermissionssection in the right pane.
- If the user for which you would like to set permissions is not listed in thePermissionssection, add it by clicking the circled plus icon at the top right of the pane.
- Select the user or group and expand thePermission operationssection.
- Allow or deny permissions, as needed.
Administration | Allows you to manage operations related to the domain organization in terms of folders and access control. | |
Access User Accounts | Allows access to user profiles that are defined within folder paths and sub-paths for which the permission is given. | |
Manage User Accounts | Allows permission assignments and creation, editing and deletion of user accounts. | |
Manage Folders | Allows you to create, edit, move, and remove folders. | |
View Connection Audit | Allows access to the connections log. | |
View Operations Audit | Allows access to the administration log. | |
Network Security | Allows you to manage the firewall configuration. | |
Device Installer | Allows you to manage devices within a specific domain. | |
Interactive Access | Allows you to interact with the remote device as a viewer and/or with read and write rights. | |
View the Desktop | Allows the Remote Desktop view only, whereas interaction is not allowed. | |
Interact with the Desktop | Allows full Remote Desktop interaction. | |
Network Access (VPN) | Allows VPN activation and subnetwork access. The subnetwork access can be filtered by applying firewall policies. | |
Passthrough (Serial + USB) | Allows to use a serial pass-through function (this option is subject to VPN activation). | |
Read Remote Files | Allows you to read files from the remote system through the Explorer section in the Interactive Access Tool. | |
Write Remote Files | Allows you to write files to the remote systems through the Explorer section in the Interactive Access Tool. | |
Chat | Allows the use of the chat through the Remote Desktop section in the Interactive Access Tool. | |
System and Processes | Allows you to access the remote processes viewer and possibly restart them as needed through the End process button in the Interactive Access Tool. |
Provide Feedback