FactoryTalk Remote Access Manager
FactoryTalk Remote Access Manager
The
FactoryTalk Remote Access Manager
consists of a web interface that allows you access a domain and interact with remote devices, such as routers, HMI terminals or IPCs that you wish to control. Furthermore, the FactoryTalk Remote Access Manager
allows you to manage domain users and their permissions, and remote devices, including their registration, connection, setting, etc.You need to create a user account first, by registering your email on the
MyRockwellAutomation webpage
to access the FactoryTalk Hub
.Once you have logged on to the
FactoryTalk Hub
, you can access FactoryTalk Remote Access
.
NOTE:
See FactoryTalk Remote Access Manager Authentication and Create an organization and a domain for further information on this subject.
Provide Feedback