- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Edit a trend
Trending in the
Logix Designer
application lets you view data sampled over a time period in a graphical display for a set of up to eight data elements. Edit currently configured trends as needed to refine the data displayed.To edit a trend:
- In theController Organizer, expand theAssetsfolder and theTrendsfolder, right-click the trend you wish to edit, and selectProperties.TheRSTrendX Propertiesdialog box opens.
- Make the desired changes.
- SelectOK.
Provide Feedback