- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Edit trend chart properties
Edit trend chart properties to modify the name, sampling rate, and triggers of a trend.
To edit trend chart properties:
- With your cursor in the chart window, right-click and selectChart Properties.TheRSTrendX Propertiesdialog is displayed.
- Select theHelpbutton from this dialog for detailed help on each individual tab, and for chart configuration information.
Provide Feedback