Converter Current Ref Signal Attrib
These are the current reference signal attributes associated with a Regenerative Converter.
Active Current Reference
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Get/GSV | T | Real | - | - | - | % Rated |
The Active Current Reference attribute is the commanded active current sourced by the DC bus voltage control loop or the Active Current Command depending on Converter Control Mode. % Rated is defined as percent of the Converter Rated Input Current.
Active Current Reference - Filtered
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Get/GSV | T | Real | - | - | - | % Rated |
The Active Current Reference - Filtered attribute is the commanded active current reference signal after passing through the active current reference filters.
Active Current Reference - Compensated
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Get/GSV | T | Real | - | - | - | % Rated |
The Active Current Reference - Compensated attribute is the commanded active current reference signal after passing through the AC Line Filter Compensation block.
Reactive Current Reference
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Get/GSV | T | Real | - | - | - | % Rated |
The Reactive Current Reference attribute is the commanded reactive current output of the Reactive Power Control block and the rate limited Reactive Current Command.
Reactive Current Reference - Compensated
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Get/GSV | T | Real | - | - | - | % Rated |
The Reactive Current Reference - Compensated attribute is the commanded reactive current reference signal after passing through the AC Line Filter Compensation block.
Provide Feedback