Standard Initialization Faults

This table defines a list of standard faults associated with the Initialization Faults attribute.
Standard Initialization Fault Descriptions
Bit
Fault
Description
0
Reserved
This bit cannot be used since the Fault Code is defined by the associated fault bit number and Fault Code of 0 means no fault condition is present.
1
Boot Block Checksum Fault
Checksum or CRC error for Boot Block of CIP Motion device detected as part of Self-Test.
2
Main Block Checksum Fault
Checksum or CRC error for Main Block of CIP Motion device detected as part of Self-Test.
3
Nonvolatile Memory Checksum Fault
Checksum or CRC error for NV Memory of CIP Motion device detected as part of Self-Test.
4...31
Reserved
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.