About the Controller/Project Status Tray

The controller/project status tray is located at the right end of the status bar. It contains icons representing the following controller status:
  • Locked
    - This icon appears when you are online. It appears differently for each of the three states of the controller lock: Locked by You, Locked by Another User, or Not Locked.
  • Project Contains Uploaded Changes
    - This icon appears whenever the project contains changes uploaded from the controller. This icon also animates during correlation.
    TIP:
    You can right click any of the icons to bring up a context menu with common commands. You can see a tooltip describing the icon state by passing your mouse over the icon.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.