Invalid rung number. Please enter a number from 0 to <number of rungs in the routine>, or the word End.

This message appears when OK is pressed, and the rung number entered is either invalid or not within the valid range.
Enter a rung number between 0 and the number of rungs in the routine.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.