- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Containers
Use container objects to structure your application and create user interface navigation.
Object | Description |
---|---|
Container for objects that constitute a specific widget. By default, each new
panel has a fixed width and height and is aligned with the top-left corner of the
parent object. | |
Container for objects that constitute a specific interface. By default, each new
screen stretches to cover the entire parent object. | |
Container that automatically arranges objects horizontally next to each other. | |
Container that automatically arranges objects vertically next to each other. | |
Container that arranges objects in a grid. | |
Container that automatically scales its children objects when the container
aspect ratio changes. | |
Container that displays other panels based on the application logic. | |
Container that contains other panels and automatically organizes panels into tabs that you can navigate. | |
Button that opens and closes a panel when selected. | |
Root container. In a Presentation Engine, you can set Window to specify the initial user interface at runtime. | |
A modal window that does not allow interaction with other interface components until it is closed. | |
Panel that can scroll to display content larger than the panel size. | |
Container that includes expandable content blocks. |
container
Provide Feedback