- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Screen
Use screens to group objects that comprise a specific interface.
Screen types and instances
For optimal project maintainability, create screen object types and then use them with panel loaders or navigation panels. This allows you to modify all screen instances by editing the parent screen type.
Screens folder
Rockwell Automation
recommends creating screen types in the folder in Project view
. You can also create screen types in different nodes of your project, for example in the UI folder.Each new project contains an empty
Screens
folder.
TIP:
If the project does not contain a
Screens
folder, see Add a Screens folder.screen
Provide Feedback