Delete items from the Controller Organizer
Use the
Delete
command to remove an item from the Controller Organizer
. Deleting an item also deletes its descendants (defined in the Logical Organizer
).
TIP:
If FactoryTalk Security is enabled, FactoryTalk Security permissions are required to create and delete items in the
Controller Organizer
and the Logical Organizer
.Before you begin:
If the controller is online, satisfy these conditions before deleting an item.
Items | Conditions |
Task | No programs are scheduled for the task. |
Program | The controller is not locked or in Hard Run mode. The program and all of its descendants do not have safety restrictions. The program does not have redundancy restrictions or security restrictions. |
Routine | Cannot delete a routine if:
|
Motion Group | No preliminary steps required. When a motion group is deleted, any axes assigned to the motion group are moved to the Ungrouped Axes branch. |
Axis | No preliminary steps required. |
User-Defined Data Type | The UDT is not referenced. The controller is not in Hard Run mode. |
I/O Module | Modules that are referenced by program logic cannot be deleted while online. To delete a module that is referenced by program logic, either remove the reference to the module or go offline and delete the module.
TIP:
When the controller is offline, a module with child modules can be deleted without first deleting the child modules. The child modules must meet these criteria:
|
Drive Module | No preliminary steps required. |
Add-On Instruction | Controller is offline. |
To delete an item from the Controller Organizer
- Right-click the item, and then chooseDelete.
- ChooseYesto confirm the deletion.TIP:Can also delete an item by selecting it and then using one of the following methods:
- From theMenubar, selectEdit > Delete.
Press theDeletekey.
For additional delete actions and information about the
Controller Organizer
, see:Provide Feedback