Use the Controller Organizer

Use the Controller Organizer

The
Controller Organizer
is a graphical representation of the contents of your project. In the
Controller Organizer
, you can:
  • Use tasks, programs, and routines
  • Reference an existing tag
  • Create a motion group and a motion axis
  • Use trends
  • Delete a task, program, tag, trend, or routine
  • Add a routine to a program
  • Cut, copy, paste, and drag commands
  • Add and edit tags and parameters
  • Add and edit routine logic
  • Add configured alarms for tags
  • Navigate from a program in the
    Controller Organizer
    to the same program or in the
    Logical Organizer
For information about other graphical representation of content, see:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal