Sub-Area Level Dashboard

Sub-Area Level Dashboard

In this dashboard, the user can view the configured hierarchy lists. Based on the configuration, respective KPI details are displayed in the
Overview
tab in the form of cards.
Select the required
Subarea
from the hierarchy list and the following tabs are displayed in the dashboard:
  1. Overview
  2. Assets
NOTE: To change the date or time period, refer to Change Date or Time Period.
Overview
The user can view the status of the Subarea and the configured KPIs across the application under the selected Subarea and the top five underperforming assets on the selected time frame. You can also view the active alerts with severity, actions taken, and the current status of the alert.
Summary Chart
In the KPI trend chart, three lines indicate the three different KPI data, the solid lines indicate the historic data, and the dotted line indicates the extrapolated future projected data. Hover over the solid line and dotted line to view the KPI values with the corresponding date.
In the KPI trend chart, the user can view the Trend at the top and a sparkline view below. The user can change the date selection by using the selectors of 1/3/6 months, year to date [YTD], 1 year, and all. The user can use the sliding selector at the bottom to change the date selection.
NOTE:
  • Click the [] icon in the chart and click
    Download SVG vector image
    to download the chart in SVG vector image format.
  • Click the [] icon in the chart and click
    View in full screen
    to view the chart in full screen.
The user can view the individual KPI graph of the
Top 5 Underperforming Assets
and the graph is displayed for the past 3 months. Hover the mouse over the chart to view the selected KPI value with the corresponding date. The user can also select the required KPI from the KPI drop-down list and the corresponding graph are displayed in the
Past 3 Months
column.
Top 5 Underperforming Assets
NOTE: To customize the top 5 underperforming asset table, refer to Customize Top 5 Underperforming Assets Table.
Click the [] icon on the required
Asset Name
to view the
Asset Hierarchy
details.
Asset Hierarchy Details
The user can view all the active alerts with alert descriptions, severity, start date, action taken, and current status details.
Active Alerts
NOTE: To customize the table, refer to Customize Table.
Assets
The user can view summaries of the asset classes associated with this point in the hierarchy. Each card represents an Asset Class with rolled-up statuses. By selecting an individual
Asset Class
, the user can filter the list of assets available in the
Asset Details
section. Click on the
Asset Name
to view the corresponding Asset page.
Asset Cards and Details
NOTE: To know about the card functionality, refer to Card Functionality.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal