Menu Bar
The menu bar on Data Explorer provides text-based selection many of which overlap with the Tool Bar options.
- Project - provides options to deal with the current or desired Data Explorer project file
- Edit - information about how the content is managed
- View - tools to help manage product windows
- Dataset - include primary manifest dataset property access, but also tools when the data spreadsheet is open
- Help - provides access to help contents including Users Guide and Tutorial
Provide Feedback