Dataset and Spreadsheet

Dataset and Spreadsheet

  • Spreadsheet - opens the current dataset as a spreadsheet or data table. Some minimal functionality is currently supported to work through the data table directly.
  • Transforms -opens the list of active dataset transforms for view or modification. Same as the Transform button on the Manifest sheet.
  • Time Merge -opens the Time Merge wizard to apply or edit existing Time Merge transforms on a dataset. Same as the Time Merge Button on the Manifest sheet.
  • Configure Properties -opens selections to label trends with additional properties imported with the dataset.
  • Reorder Columns -opens the current dataset variable list which may be reordered here.
    Dataset
  • Find Row is active only when the Spreadsheet is open and active and moves to a selected row in the spreadsheet.
  • Manage Variables (when spreadsheet is open and active) supports selecting alternative or additional variables or sorting them.
  • Set Displayed Columns (when spreadsheet is open and active) supports selecting columns by name using a string filter.
  • Sort - allows (one time) dataset column labels to be sorted. Same as the Reorder Column button on the Manifest sheet.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal