Tool Bar

Tool Bar

The main Data Explorer tool bar has the following icons:
Icon
Description
To display and manage a list of imported datasets as well as artifacts saved in the project including filters, analyses, plots, and exports.
To paste the copied data.
To paste the copied data.
To select all the data displayed in the UI.
To import data from an XLS or CSV file, add new variables or rows and link to a Pavilion8 dataset, or export your dataset or select variables to develop a Virtual Online Analyzer model.
Click the drop-down menu in the
Dataset
icon to open an imported dataset, spreadsheet, transforms, or time merge configure custom dataset properties or reorder dataset variables.
Click the drop-down menu in the
Plot
icon to select a type of plot to display. Any mapped dataset variable may be added to a display. Alternatively, you can also select a new plot to display by right-clicking on the viewed content data and selecting
Plot
> <plot_type>.
Click the drop-down menu in the
Analysis
icon to select a
type of analysis to display. Any mapped dataset variable maybe added to a display. Alternatively, you can also select a new
plot to display by right-clicking on the viewed content data and selecting
Analyze
> <analysis_type>.
To define and apply highlighting rules, reset a highlighter, or convert it to a filter.
Most highlighting activities are done directly within plots, but highlighting editing or management is executed with options under the
Highlighter
icon. See“Highlighting Data” on page 59 for more details
Click the
Filter
icon to create a new or edit an existing dataset filter. See“Filtering Data” for more details.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal