Raw vs Transform Plots

Raw vs Transform Plots

Raw vs Transform plots displays data using both the raw data and transformed data. If the selected variable is a raw variable (as defined in “Data Preparation”), then this plot shows two traces on the same pair of axes, the before-transforms values and the after-transforms values, so you can see the effect of the transforms. If there are no transforms on this variable, then the two traces will be identical. However, if the selected variable is not raw, then it does not have any before-transforms values, and this plot shows only one trace, the after-transforms values.
For example, suppose that Unit 2 O2 and NOx are process variables that have noisy measurements.
Raw vs Transform Plot Example
You can apply a moving average transform to smooth out the noise.
Smoothing Configuration
The Raw vs Transform plot now shows the original data (blue) and the smoothed data (red). Note that if there is no transformation on a variable only one color will be visible as they exactly overlay each other (raw and transformed variables).
Raw vs Transform Plot
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal