arx(var, D, b0, b1, …, bN-1, a1, a2, …, aN, mode)

arx(var, D, b0, b1, …, bN-1, a1, a2, …, aN, mode)

This transform implements a causal linear filter of arbitrary degree with dead-time. The equation implemented is
res[t]=-a1[t]*res[t-1]-a2[t]*res[t-2]-…
+b0[t]*var[t-D]+b1[t]*var[t-1-D]+…
such that var[t] is the filter input, res[t] is the filter output, D is a constant integer delay, and the parameters ai and bi are either constants or variables (within the artifacts tabs, this is accessible directly as the Transform > Dynamic Filter option).
The filter degree, N, is inferred from the total number of arguments with the assumption that an equal number of a and b parameters is specified. To implement an unbalanced transfer function, the value 0.0 is specified for unused parameters. There is no restriction against specifying unstable filters. If a Break status is encountered in either var or one of the parameter variables as part of transform evaluation, the filter is put into an off-line state. This state propagates a Break status to the output and requires that the filter be re-primed before normal filtering resumes. This re-priming occurs automatically when both var and the parameters return to OK status and causes the internal filter states to re-initialize to steady-state values consistent with the new input value var[t]. Note that if the filter parameters define any discrete time poles at z=1 (embedded integrators), the steady-state condition of the filter has all internal states set to 0.0.
The mode argument is used to control processing of Error statuses; it can be FILTER_DISABLE or FILTER_SMOOTH. FILTER_DISABLE causes the filter to go off-line and propagate the Error status to the output. This is the typical mode used during signal shaping and noise filtering applications where errors are not a systematic part of the process. FILTER_SMOOTH is more applicable when frequent errors are expected as part of normal behavior, such as when a set of sparse lab measurements occurs with intervening error values. In this mode, the filter returns an OK status and attempts to filter smoothly over the error condition.
Examples:
  • Causal Shift
    : A causal shift can either be performed using the D term as in
$shift(!x!,1) == $arx( !x!,1, 1, 0, $FILTER_DISABLE )
$shift(!x!,2) == $arx( !x!,2, 1, 0, $FILTER_DISABLE )
or using the b terms as in
$shift(!x!,1) == $arx( !x!,0, 0,1, 0,0, $FILTER_DISABLE )
$shift(!x!,2) == $arx( !x!,0, 0,0,1, 0,0,0, $FILTER_DISABLE )
  • Prev
    : The $prev transform is not really an operator like shift but an accessor of a previous row of the output of the transform. Its equivalent using ARX would be context dependent.
  • Non-Causal Shift
    : Non-causal transforms such as $shift(x,-2) are not representable using ARX. However, most of the on line uses of non-causal $shift are used to get around the state problem. Furthermore, non-causal shift is usually not as problematic on-line as the causal shift.
  • Delta
    : The $delta(!x!,1) transform is also non-causal since it computes
y[k] = x[k+1] - x[k]
Here, we need to use two transforms. First use ARX to maintain correct state at the beginning of the table, followed by shift to provide the non-causality:
!y1! = $arx (!x!,0, 1,-1, 0,0, $FILTER_DISABLE )
!y2! = $shift (!y1!, -1 )
  • Integrator
    : The ARX filter can also be used to simulate an integrator:
!intx! = $arx (!x!,0, 1, -1, $FILTER_DISABLE )
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal