Common Transforms and Constants

The following is a list of common transforms and constants.
NOTE:
The orange colored Transforms from the following list cannot be translated by Data Explorer into a streaming equivalent. This maybe because the transform is non-causal or that it manipulates entire columns as single operand to generate a single summary value. When a transform's causality is mode dependent, then the causal modes are supported (e.g. $lag option in moving filters).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.