error

error

This function has no input argument; it simply returns a point with Error status. Generally, it is used as the value resulting from a Conditional Expression (see “Conditional Expression Constructors”). It can be applied to a variable of any type.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal