delta(var[,n])

delta(var[,n])

The two arguments are a variable and an integer n. The second argument may be omitted and then defaults to be 1. If n>0, the result is the value of the specified variable in row current+n minus the value in the current row; if n=0, the result is undefined; if n<0, the result is the value of the specified variable in the current row minus the value in row current+n; except that, if row current+n is beyond a cell with Break status, or beyond the end of the column, then the result is zero. See Transform Combination Restrictions.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal