fft(var,length)

fft(var,length)

Calculates a raw Fast Fourier Transform (FFT) with no data windowing or concern about aliasing. You specify an input variable and a length which must be a constant power of 2. The input variable must not have any invalid points. This special transform requires a list of up to five output variables (that correspond to the frequency, real, imaginary, magnitude, and phase values), as described in “Transforms With Multiple Outputs”.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal