holdLast(var
[,num_cycles])
If variable var has a bad status, use the last good value for var instead. If you
do not specify the optional num_cycles argument, the last good value is used indefinitely, or
until status returns to good. If you specify the num_cycles argument, the last good value is
used for at most that number of execution cycles or until status returns to good, whichever
comes first. See Transform Combination Restrictions.
Provide Feedback