left(x,n) or left(x,characterList)

left(x,n) or left(x,characterList)

The first argument is a variable or value of any type. This function converts the first argument to a string (if it is real or double, it is formatted with six decimals only); then either extracts the leftmost n characters from the string, where n is a positive integer constant; or extracts all characters to the left of any character in the specified characterList, where characterList is one or more characters listed within quote (") characters. The output is a string variable. For example,
$left ("abcdefg",4) = abcd
$left("abcdefg","cxn") = ab
If nothing in the characterList is found in the string, the result is the entire input string.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal