lookupRel(var1,var2)

lookupRel(var1,var2)

This relative lookup function returns the value of the first argument in a row number calculated by adding the values of the second argument to the current row number. The first argument can be of any variable type. Note that both arguments must be variables. For example, suppose there is a variable called !key!, and its values in the first four rows of the dataset are 3, 27, 49, 31; if you type the transform
$lookupRel(!flow1!,!key!)
then the results in the first four rows of the dataset will be the original values of !flow1! from rows 4, 29, 52, and 35.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal