break(x)
Sets the output point to the specified value but with Break status; generally used as the value resulting from a Conditional Expression (for more information, see“Conditional Expression Constructors”). The input value can be a numeric or date/time variable or constant, but not a string; use $changestat to change the status of strings.
Provide Feedback