midn(string,length,numStart)

midn(string,length,numStart)

Returns a portion of the string beginning at character number numstart and ending with character number numend, where numstart and numend are positive integer constants. If this segment is beyond the length of the input string, the result is an empty string, not an error. The output is a string variable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal