movegauss(var,size[,alignment[,stddev[,threshold]]])

movegauss(var,size[,alignment[,stddev[,threshold]]])

Gaussian filter applied within a moving window. The standard deviation argument must be a positive constant. NOTE that the $lead and $lag versions of this function are simply shifted versions of $center response. This is not the standard behavior for a moving Gaussian average and does not weight the current input sample most heavily. See also Moving Window Transforms.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.