override($self,startrow,[endrow,]value)
Changes the input
variable to a value in all rows from startrow through endrow; if
the optional endrow is omitted, it is assumed to be the same as
startrow. The output variable must be the same as the input variable.
Provide Feedback